DOCA0172EN-21

Modbus Registers Tables

Presentation

The Modbus registers of EcoStruxure Panel Server and the Modbus registers of the supported wireless devices connected to it provide measurement and monitoring information.

The Panel Server provides a consolidated table (Synthesis table) of information from all connected wireless devices at once. The content of the table is built dynamically; a maximum of 100 wireless devices are listed in the table organized by virtual server ID.

The address of the synthesis table (247 by default) can be configured at Settings > Wireless devices > Global functional settings (for details).

For detailed information about these Modbus registers, refer to DOCA0241EN EcoStruxure Panel Server - Modbus File.

Table of Modbus Functions

The following table describes the functions supported by the Panel Server to read and/or write data on the Modbus registers of wireless devices.

Function code

Function name

03

Read n words

16

Write n words

100-4

Read n non-adjacent words where n ≤ 100 (refer to Function 100-4: Read Non-Adjacent Registers)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.