DOCA0184EN-07

Information on the Products in the Panel

By selecting either the entire enclosure or a device or a group of devices, the product descriptions are displayed in the properties section, which are grouped into three categories:

  • Enclosure

  • Installation system

  • Devices and distribution blocks

To get the detailed information and documentation is available for each product by clicking on the link product data.

A mouse over a product mounted inside the panel allows to have the designation of this element defined in the diagram.

A left-click on a product makes a blue frame appear around the concerned and a black frame around the upstream device. This upstream-downstream identification function operates also for the products sorted in the workbench.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.