DOCA0106EN-16

IMU Information

Description

The IMU Information page gives the information about the devices connected to the ULP port of the EIFE interface. The devices connected are:

  • MicroLogic X control unit

  • IO module IO 1

  • IO module IO 2

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.