DOCA0106EN-16

SNMP Parameters

Manage IP Parameters

The EIFE interface supports SNMP, allowing a network administrator to access remotely an EIFE interface with an SNMP manager and to view the networking status and diagnostics of the EIFE interface in the MIB-II format.

Parameter

Description

Setting

Manager One

Allows you to configure the IP address of SNMP manager one.

–

Manager Two

Allows you to configure the IP address of SNMP manager two.

–

System Contact

Allows you to configure the SNMP system contact name.

–

System Name

Allows you to configure the system name.

–

System Location

Allows you to configure the SNMP system location.

–

Read-only Community Name

Allows you to configure the SNMP read-only community name.

Public (default setting)

Read-write Community Name

Allows you to configure the SNMP read-write community name.

Private (default setting)

Trap

Allows you to trap the community name.

Alert (default setting)

NOTE: Only SNMP version 1 is supported.

Enabled Traps

Parameter

Description

Setting

Coldstart Trap

Generates a trap when the EIFE interface is powered ON.

–

Warmstart Trap

Not supported

–

Linkdown Trap

Generates a trap when an Ethernet port communication link is disconnected.

–

Linkup Trap

Generates a trap when an Ethernet port communication link is reconnected.

–

Authentication Failure Trap

Generates a trap when an SNMP manager is accessing the EIFE interface with incorrect authentication.

–

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.