DOCA0106EN-16

Webpage Access

Group Access

Group

Access

Administrator

Full access to all webpages.

NOTE: It is recommended to change the default administrator password for system security the first time you log in.

Guest

Read-only access to selected webpages.

User-defined groups

Choosing from the following options, the administrator assigns webpage access for each group. The access levels are as follows:

  • None: A group has no access to selected webpage

  • Read-Only: The password grants a group read-only access to the selected webpage

  • Full: A group has the same access as the administrator group to the selected webpage

NOTE:
  • The Webpage Access is available for the Administrator only.

  • The Administrator has full access to all the webpages.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.