DOCA0106EN-16

EIFE

Description

The EIFE page displays the information of the EIFE interface connected to the circuit breakers.

The users with installer or engineer roles can change the Diagnostics page settings.

Navigation to the EIFE Page

To view the EIFE page, click DIAGNOSTICS > EIFE.

EIFE Interface Parameters

Parameter

Description

Serial Number

Device serial number

Commercial Reference Number

Device commercial reference number

Firmware Revision

Current firmware version

Unique Identifier

Combination of MAC address and the time

MAC Address

Unique MAC address

IPv4 Address

IPv4 address of the EIFE interface

IPv6 Link-local Address

IPv6 address used to communicate on the local network

Date and Time Parameters

Parameter

Description

Time Source

Source of time with which the last synchronization has happened

Last Synchronization

Elapsed time from last synchronization

NTP Synchronization Status

Status of NTP Synchronization

NTP Stratum

Describes the accuracy of NTP time. It can take values from 1 to 15 or as NA (not applicable) if NTP server is not reachable.

File System Parameters

Parameter

Description

Total Size

Total amount of the EIFE interface disk size in kilobytes

Used Size

Total amount of used disk size on the EIFE interface disk in kilobytes

Free Size

Total amount of unused disk space on the EIFE interface disk in kilobytes

Bad Size

Amount of corrupted disk space on the EIFE interface disk in kilobytes

System Parameters

Parameter

Description

CPU

Status of the CPU:

  • Nominal

  • Degraded

  • Out of service

Boot Memory

Status of the boot memory

EEPROM

Status of EEPROM

File System

Status of the file system

Ethernet PHY 1

Status of PHY 1 hardware

Ethernet PHY 2

Status of PHY 2 hardware

DDR

Status of the execution memory

EIFE Interface Operating Time Parameters

Statistic

Description

Operating Time

Operating time of EIFE interface

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.