DOCA0106EN-16

IP Network Services

Description

The IP NETWORK SERVICES page allows you to set and activate the IP network services.

The users with Security Administrator role can edit the IP network services parameters.

Navigation to the IP Network Services Page

To view the IP NETWORK SETTINGS page, click SECURITY > IP NETWORK SERVICES.

IP Network Services Parameters

Parameter

Description

Value

Modbus TCP

Allows you to enable/disable the Modbus/TCP service.

Default setting: Enabled

Secure Commissioning

Allows you to enable/disable the secure communication over TLS and then by RBAC mechanism between EcoStruxure Power Commission software and EIFE interface.

NOTE: It is recommended to set it as Enabled. Once the secure commissioning is enabled, if EcoStruxure Power Commission software is connected to EIFE interface, user must start a new discovery of the EIFE interface with EcoStruxure Power Commission software.

Default setting: Disabled

Allows you to set the port number of the secure commissioning server.

Setting range:1...65534

Default setting: 49152

Secure Modbus for M2M

Allows you to enable/disable the secure Modbus for machine-to-machine service.

NOTE: Machine-to-Machine secure communication requires components that connect to the EIFE interface to support the Secure Modbus communication.

Default setting: Disabled

Allows you to set the port number of the secure Modbus server.

Setting range:1...65534

Default setting: 802

Allows you to set the number of sessions for the secure Modbus server.

Setting range:1...8

Default setting: 2

Internal FTPS Server

Allows you to enable/disable the FTPS server.

Default setting: FTPS server is disabled

Discovery

Allows you to enable/disable the discovery (DPWS) of the EIFE interface automatically.

Default setting: Enabled

HTTP/Web Port

Allows you to set the port number of the HTTP/Web server.

Setting range:1...65534

Default setting: 80

HTTPS Port

Allows you to enable/disable the HTTPS service and to set the port number of the HTTPS server.

NOTE: After disabling the HTTPS, you should clear the browser cookies before authenticating it again.

Setting range:1...65534

Default setting: Enabled (value: 443)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.