DOCA0106EN-16

SNMP

Description

The SNMP page displays the diagnostic data of SNMPV1 Agent parameters.

The users with installer or engineer roles can change the Diagnostics page settings.

Navigation to the SNMP Page

To view the SNMP page, click DIAGNOSTICS > COMMUNICATION > SNMP.

SNMPV1 Agent Parameters

Parameter

Description

State

Displays the state of SNMPV1 agent.

Received Packets

Number of packets received from the network.

Emitted Packets

Number of packets transmitted from the network.

Emitted Traps

Number of traps transmitted on detection of a change as asynchronous notification from agent to manager.

Received Bad Community Names

Number of received bad community names.

Emitted Bad Community Names

Number of transmitted bad community names.

Click Reset Counters to reset the statistics values to 0.

If the EIFE interface is switched off or if it is reset due to a configuration change or another event, the statistics values are reset to 0.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.