ESXP2GE019EN-05

Application Outcomes

Protection Schemes

Intelligent Electronic Devices (IED) monitor and help protect electrical distribution systems with all required features, including:

  • Thermal overload protection

  • Generator protection

  • Transformer protection

  • Arc flash protection

Automation Schemes

  • Fast Self-Healing: detects, isolates and restores the power in MV open loop electrical topologies in less than 300 ms.

  • Automatic Transfer Switch / Power Transfer Switch: automatically switches to backup power in the event of a fault on the primary source.

  • Load-shedding: keeps critical loads connected while shedding non-critical ones to balance generation and consumption.

  • Load-restore: limits the inrush current while reconnecting the loads by sequentially reclosing power transformers.

  • Emergency Genset Capacity Management: balances the emergency genset's capacity with the energy consumption according to the available power.

Live Data Display

  • Animated Single-Line Diagrams (SLD) display the status of the system with color animation to distinguish sections with and without a power supply.

Events and Alarms

  • System events and alarms are displayed in chronological order with sorting and filtering capabilities.

Trends

  • Real-time and historical data can be viewed on a trend viewer.

Remote Control

  • Select-before-operate commands are available from SCADA HMI.

Cloud-Based Analytics and Service

EcoStruxure Service Plan powered by EcoStruxure Asset Advisor provides remote monitoring, asset management consulting and on-site maintenance activities with recommendations from our Schneider Electric service experts.

It includes:

  • Continuous asset monitoring and alarms with remote notifications in the event of electrical asset condition anomalies

  • Predictive analytics to help determine remaining equipment lifetime and other health indicators

  • Condition-based asset maintenance triggered by a Maintenance Index

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.