ESXP2GE019EN-05

Data Recording and Timestamping

All protection, automation, and control system activities are recorded and timestamped for postmortem analysis, traceability, and auditing.

For critical applications, a timestamp accuracy of ±1 ms is required to help ensure a correct sequence of events.

To achieve this, the measurements and events are recorded and timestamped onboard smart equipment such as PowerLogic P5/P3 and C5 and EcoStruxure Power Automation System Gateway.

For a comprehensive overview of device recording and timestamping capabilities, refer to Data Recording and Time Synchronization Capabilities of EcoStruxure Power Connected Products.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.