ESXP2GE009EN-05

Data Processing

The recorded energy data is converted to energy cost using the information in the rate file. It is then allocated to tenants, areas, departments, or buildings based on the metering hierarchy.

Cost allocation data processing is embedded in the optional Billing Module of EcoStruxure Power Monitoring Expert or Power Operation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.