ESXP2GE016EN-05

Digital Architecture

The digital architecture of the Circuit Breaker Settings Monitoring application depicts the collection of the protection settings of different circuit breakers via gateways (Enerlin'X IFE, eIFE, or IFM). These data are then recorded and processed by the Edge Control software (EcoStruxure Power Monitoring Expert or Power Operation) for on-premise visualization, analysis, and reporting.

The recommended digital architecture for the application is shown below:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.