ESXP2GE011EN-05

Inputs

The following data are acquired during the manufacturing and commissioning of electrical assets:

Asset Information and Maintenance Schedules

  • Electrical characteristics and serial number are captured as per nameplate, as well as context information that will help locate the Asset (customer, country, town, facility, building, floor, etc.).

  • Maintenance templates and schedules include the standard manufacturer recommended maintenance procedures and schedules for a given electrical asset.

  • Standard templates exist for a number of electrical assets such as:.

    • Medium voltage equipment (PremSet, SM AirSeT, PIX)

    • Low voltage equipment (PrismaSeT, Okken)

    • Power transfer switches (ASCO 7000 Series PTS)

    • Motor control centers

    • Circuit breakers such as MasterPacT MTZ, ComPacT NSX, and Acti9 iC60

    • Power correction devices such as PowerLogic PFC and AccuSine

    • Trihal transformers

  • For non-native equipment, templates can be created in EcoStruxure Facility Expert.

Asset Documentation

Asset documentation produced during panel construction can be attached to a defined electrical asset. This documentation may include wiring diagrams, single-line diagrams, user documentation, bill of materials, device serial numbers, and more. Documentation is stored digitally, accessible through the EcoStruxure Facility Expert app, and maintained as necessary during the operational life cycle.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.