ESXP2GE011EN-05

Outputs

Outputs are displayed remotely via EcoStruxure Facility Expert software.

Dashboards

Map View

EcoStruxure Facility Expert provides a map view of where electrical assets are located.

  • By clicking on a particular site, the list of the electrical assets can be viewed.

  • Selecting an electrical asset provides access to its preventive maintenance status, procedures, and documentation.

  • The available documentation consists of test reports (electrical, communication, etc.), electrical drawings, bill of material (BOM), etc.

  • Users can also identify the required maintenance tasks and assign them to the appropriate person or team.

Reports

Facility Expert Maintenance Report

Maintenance reports can be generated to easily identify a summary of the status of maintenance tasks for electrical assets.

For a given asset, it provides:

  • nameplate information

  • key information including maintenance logs over the selected period, list of performed tasks, duration of inspections, and maintenance contributors

  • visualization of all late or upcoming maintenance tasks

Maintenance Plan

Maintenance plans with auto-generated templates for Schneider Electric assets can be generated.

Notifications

The EcoStruxure Facility Expert application provides alerts and notifications when preventative maintenance tasks are due.

Alarm details and relevant associated actions such as acknowledgement, planning, and assignment of tasks are instantly accessible from the notification.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.