ESXP2GE002EN-05

Inputs

The following data are required to implement the Energy Monitoring application.

Electrical Measurements

The following electrical measurements are collected at each point of interest in the electrical distribution, from Medium Voltage, to Low Voltage, down to Final Distribution.

  • Power values (kW, kVAR, kVA)

  • Energy values (kWh, kVARh, kVAh)

These data may be acquired from:

  • Third-party devices (via Modbus)

Other Utility Consumption Inputs

The following utilities can be monitored:

  • Water

  • Air

  • Gas

  • Steam or heat flow

They can be acquired via digital/analog inputs on meters or directly via Modbus from third-party devices.

Tarrifs (User Input)

To convert energy consumption into cost, it is necessary to apply the relevant tariffs to the power/energy consumption values.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.