ESXP2GE025EN-05

Digital Architecture

In this architecture, the combined power factor measured at utility entrance is collected from connected products (PowerLogic ION9000 or PM8000) directly over Ethernet and then recorded and processed by the Edge Control software (EcoStruxure Power Monitoring Expert or Power Operation) for on-premise visualization, analysis, and reporting. Communications are performed directly over Ethernet for PowerLogic AccuSine EVC+ and through a Modbus Serial connection for PowerLogic PFC. EcoStruxure Panel Server gateway converts the Modbus communications to Ethernet for real-time data acquisition by the Edge Control software (EcoStruxure Power Monitoring Expert or Power Operation).

As an option, data from EcoStruxure Power Monitoring Expert or Power Operation can be passed on to the EcoStruxure Power Advisor platform and analyzed by experts as part of the EcoStruxure Service Plan.

The recommended digital architecture for the application is shown below:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.