ESXP2GE025EN-05

Data Recording and Timestamping

For power factor correction equipment, data recording is performed by EcoStruxure Power Monitoring Expert or Power Operation, based on real-time values acquired by the driver. For the power quality meters located at the service entrance, data recording is performed on board the device(s). For these device(s), a time accuracy of 1 second or better is recommended.

For a comprehensive overview of device recording and timestamping capabilities, refer to Data Recording and Time Synchronization Capabilities of EcoStruxure Power Connected Products.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.