ESXP2GE025EN-05

Inputs

The following data is required:

Electrical Measurements and Parameters

  • Power Factor (measured and targeted)

  • Other electrical measurements: voltage, current, frequency, power (kW, kVAR, kVA), harmonics

A power meter (PowerLogic ION9000 or PM8000) at the utility entrance is used to check that the combined power factor, as seen by the utility, is within allowable thresholds to avoid power factor penalties.

Status and Diagnostic Information for the Capacitor Bank

  • Active compensation steps

  • Broken steps

  • Step power loss

  • Hunting

  • Over/under compensation

  • Temperature

  • THD voltage, voltage tolerance, overcurrent

  • Switching cycles

  • Operating hours

  • Ambient and max temperature

  • Capacitor overload

  • Fan status

This information is acquired by Power Factor Correction equipment such as PowerLogic PFC/AccuSine EVC+.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.