ESXP2GE025EN-05

Outputs

Live data, alarms, events, and dashboards are available by default in EcoStruxure Power Monitoring Expert and Power Operation.

Live Data Display

Live data acquired by the software driver can be displayed in Power Monitoring Expert or Power Operation through equipment diagrams.

The real-time data displayed include electrical measurements, operating modes, statuses, and maintenance indicators.

Events and Alarms

Events and alarms are generated by the Edge Control software upon change of the statuses. The events are timestamped by the PC, recorded, and displayed in the software’s default alarms interface as diagnostic alarms.

Trends

All analog values stored as historical data can be displayed as trends to monitor their evolution over time.

Dashboards *

Electrical parameters acquired and recorded natively by power factor correction equipment (PowerLogic PFC and PowerLogic AccuSine EVC+) can be displayed as historical data in dashboards. Some examples of these dashboards include:

  • PF Impact

  • PF Impact Trend

Cloud-Based Analytics and Services

As an option, EcoStruxure Service Plan powered by EcoStruxure Power Advisor provides data quality analytics with recommendations from our Schneider Electric service experts.

For further information, refer to Data Quality Management.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.