ESXP2G001EN-Trans-05

Data Recording and Time Synchronization Capabilities of EcoStruxure Power Connected Products

The table below highlights the data recording capabilities and supported time synchronization methods.

Connected Product Product Category Data Recording Capabilities* Maximum Achievable Time Synchronization Accuracy / Compatible Time Synchronization Protocols* *
Event Log Measurement Log 1 ms 10/100 ms 100 ms 1 s
PTP IRIG-B NTP DCF 77 SNTP 1per10 Over Modbus Over ION
PROTECTION, MONITORING, and CONTROL DEVICES
PowerLogic P5 Advanced High          
PowerLogic P3 Advanced High            
PowerLogic C5 Advanced High              
PowerLogic T300 Advanced High            
MasterPacT MTZ (with IFE/eIFE) Advanced Limited            
ComPacT NSX (with IFE) Advanced Limited            
TransferPacT Active Advanced Limited                
ASCO 7000 Series PTS - Group 5 Controller Advanced Limited                
Acti9 Active* Basic                    
Arc V121 / PowerLogic A125* Basic                    
ASCO 7000 Series PCS - Modicon M580 Advanced High            
ASCO SPD with ASM Standard                  
ASCO CPMA Advanced Limited                  
INSULATION MONITORING and FAULT LOCATION DEVICES
Vigilohm IM20-H Advanced Limited              
Vigilohm IFL12-H/IFL12 Advanced Limited              
Vigilohm IM400 Advanced Limited              
POWER METERS
PowerLogic ION9000 Advanced High    
PowerLogic PM8000 Advanced High    
PowerLogic PM5000 Advanced Limited            
PowerLogic HDPM6000 Advanced Limited              
Acti9 iEM3000 Advanced Limited                  
PowerLogic PowerTag Standard                    
ASCO 5200 Advanced Limited                  
PLC and PAC
Modicon M251 (SMD) Advanced Limited              
Modicon M580 Advanced Limited            
Modicon M580 with ERT module Advanced High        
Modicon M340 Advanced Limited            
POWER QUALITY MITIGATION, POWER FACTOR CORRECTION, and UPS DEVICES
PowerLogic AccuSine PCS+* Standard                    
PowerLogic AccuSine PCSn* Standard                    
PowerLogic AccuSine EVC+* Standard                    
PowerLogic AccuSine PFV+* Standard                    
PowerLogic PFC* Basic                    
Galaxy VX Advanced Limited              
Galaxy VL Advanced Limited              
Galaxy VM Advanced Limited              
Galaxy VS Advanced Limited              
COMMUNICATION DEVICES, GATEWAYS, and DATA LOGGERS
EcoStruxure Panel Server PaS400 Advanced Limited                  
EcoStruxure Panel Server PaS600 Advanced Limited                  
EcoStruxure Panel Server PaS800 Advanced Limited              
Acti9 Smartlink Modbus Advanced Limited                
PowerTag Link Advanced Limited                
Harmony Sologate ZBRN32* Standard                    
EcoStruxure Power Automation System Gateway* Advanced High              
Cyber Sciences SER 3200/2408 Advanced High      
Connexium Managed Switches Advanced Limited                
SENSORS
PowerLogic TH110/CL110* Basic                    
PowerLogic HeatTag* Basic                    

For a definition of "product categories" and for more information on time synchronization and how to implement such a feature in a digital architecture, please refer to the dedicated How to Optimize Time-Synchronization and Data Recording for EcoStruxure Power Digital Applications

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.