ESXP2GE001EN-05

Application Outcomes

Live Data Display

  • Native support for a wide range of devices and communication protocols

  • Electrical network Single-Line Diagrams (SLDs)

  • SLD color animation to distinguish energized/de-energized sections

  • Elevation drawings

  • Real-time data values of each connected device, such as electrical parameters, device settings, and status information

Events and Alarms

  • Chronological display of events and alarms with sorting and filtering capabilities

  • Intelligent alarm grouping into summary incidents

Trends

  • Real-time and historical data can be viewed on a trend viewer.

Dashboards

  • Configurable dashboards for visualizing historical power system data

Reports

  • Historical data reporting

Notifications

  • SMS and/or email notifications can be sent for fast analysis and action.

  • Email notifications are also available to send reports and non-critical information.

Analysis Tools

Display of incidents on the Power Event Analysis incident timeline (for more information, refer to the Power Event Analysis application).

Display of electrical waveforms captured during arc flash event with a native waveform viewer in Edge Control software.

Cloud-Based Analytics and Services

As an option, EcoStruxure Service Plan powered by EcoStruxure Power Advisor provides electrical network and alarm health analytics with recommendations from our Schneider Electric service experts.

BMS Integration

EcoStruxure Power enables integration of electrical data and alarms at the Edge Control layer with BMS software such as EcoStruxure Building Operation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.