DOCA0151EN-12

Firmware Version 6.1.1

New Features

  • Added RBAC access management with three levels: Guest, Operator, and Administrator

  • Added the following communication settings:

    • Extended auto-discovery from single gateway to several gateways

    • Manual addition of additional single IP devices from General view

    • Communication settings displayed from General view

  • Added IMU location feature

  • Added Czech language

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.