990-5913G-001

Installation Procedure

NOTE: The distance between the battery bank and the UPS must not exceed 200 m. Contact Schneider Electric for installations with a longer distance.
  1. Prepare for Cables.
  2. Perform one of the following:
  3. Connect the Power Cables.
  4. Add Translated Safety Labels to Your Product.
  5. Final Installation.
For moving or decommissioning the classic battery cabinet after installation has been completed, please see Decommission or Move the Classic Battery Cabinet to a New Location.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.