990-91381D-001

Connect the Signal Cables Between the Maintenance Bypass Cabinet and the UPS

  1. Connect the provided Class 2/SELV signal cable 0W50021 and the provided non-Class 2/non-SELV signal cable 0W50023 between the maintenance bypass cabinet and the UPS as shown.

    Single Mains System

    Dual Mains System

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.