990-91381D-001

Prepare for Signal Cables in Top Cable Entry Systems

DANGER
hazard of electric shock, explosion, or arc flash
Do not drill or punch holes with the gland plates installed and do not drill or punch holes in close proximity to the cabinet.
Failure to follow these instructions will result in death or serious injury.
  1. Prepare the UPS for signal cables:
    1. Remove the cover.
    2. Remove the gland plates and brush plates from the top of the UPS.

      Front View of the UPS

    3. For installation without grommets: Reinstall the brush plates.
    4. For installation with grommets: Drill a hole in the gland plates for grommets, install grommets, and reinstall the gland plates.
  2. Route the signal cables as shown to separate the Class 2/SELV cables from the non-Class 2/non-SELV cables. A divider inside the cable channel separates the cables.

    Front View of the UPS

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.