990-91734A-001

Install the Busbars Between the UPS and the Output Transformer Cabinet in a Single Mains System

The busbars and insulator parts are provided in a kit with the output transformer cabinet. The part numbers shown on the illustrations are printed on the parts. Use the provided M8x30 screws and torque to 17.5 Nm (12.91 lb-ft / 154.9 lb-in).
  1. Install the neutral busbars, the DC busbars, the insulator part, and the ground busbar.

    Front View of the UPS

  2. Install the input busbars and the insulator part.

    Front View of the UPS

  3. Install the output busbars and the insulator parts.

    Front View of the UPS

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.