990-91111L-018

漏れ電流

100%負荷時の380/400/415 V UPSシステムの4線設置

UPS定格 漏れ電流
20~50 kW 62 mA
60~100 kW 67 mA
120~150 kW 91 mA
フィードバック
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.