990-91262D-031

Momentspecifikationer

Bultstorlek Vridmoment
M4 1,7 Nm (0,17 kgf-m)
M5 2,2 Nm (0,22 kgf-m)
M6 5 Nm (0,51 kgf-m)
M8 17,5 Nm (1,78 kgf-m)
M10 30 Nm (3,04 kgf-m)
M12 50 Nm (5,09 kgf-m)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.