990-91317H-001

Leakage Current

380/400/415 V UPS system 4-wire installation at 100% load

UPS rating Leakage current
10-20 kW 60 mA
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.