990-55223-001

Install the Rear Seismic Anchoring

  1. Mount the rear seismic assembly (4 x 870-50102 and M6 x 16 torx screws from accessory kit 0M-95331 and the rear shipping bracket) to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear seismic bracket is ø14 mm. The minimum requirement is M12 strength grade 8.8 hardware.

    Rear View

  2. In systems with more battery cabinets, interconnect the seismic assemblies with the interconnection plate 870-51172 from the accessory kit 0M-95331.

    Rear View

  3. Remove the indicated screws.

    Rear View

  4. Remove the rear seismic bracket.

    Rear View

  5. Install the rear seismic bracket on the battery cabinet(s).

    Rear View

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.