990-55223-001

Installation Procedure

  1. Lithium-ion battery cabinet(s): Prepare for Installation.
  2. UPS: Prepare for Installation.
  3. Only for UPS without preinstalled power modules: Install the Power Module(s).
  4. UPS: Install the Seismic Anchoring (Option).
  5. Lithium-ion battery cabinet(s): Install the Rear Seismic Anchoring.
  6. Lithium-ion battery cabinet(s): Position and Interconnect the Battery Cabinets.
  7. Lithium-ion battery cabinet(s): Install the Front Seismic Anchoring.
  8. Only for UPS for TN-C/480 V solid-grounded earthing system (no neutral connection): Prepare the UPS for TN-C/480 V Solid-Grounded System.
  9. UPS: Perform one of the following:
  10. UPS: Connect the Signal Cables.
  11. UPS: Connect the Signal Cables from Switchgear and Third-Party Auxiliary Products.
  12. UPS: Connect the External Communication Cables.
  13. UPS: Connect the Modbus Cables.
  14. UPS: Add Translated Safety Labels to Your Product.
  15. UPS: Final Installation.
  16. Lithium-ion battery cabinet(s): Install the Battery Modules in the Battery Cabinet.
  17. Lithium-ion battery cabinet(s): Connect the Power Cables.
  18. Lithium-ion battery cabinet(s): Route the Signal Cables to the Switchgear, Rack BMS, and System BMS Ports.
DANGER
hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Startup must only be performed by Schneider Electric.
Failure to follow these instructions will result in death or serious injury.

For moving or decommissioning the UPS or the Lithium-ion battery cabinets after installation has been completed, see Decommission or Move the UPS to a New Location or Decommission or Move the Battery Cabinet to a New Location.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.