990-55224-001

Overview of User Interface

Display

Overview of the Home Screen

  1. Home button - tap here on any screen to return to the home screen.

  2. Main menu button - tap here to access the menus.

  3. Mimic diagram button - tap here to access the mimic diagram.

  4. Alarm status symbol - tap here to access the active alarms log.

You can tap on the output or battery fields on the home screen to go directly to the detailed measurement pages.

Main Menu


Tap the main menu button on the home screen to access the menus.

Mimic Diagram

The mimic diagram will adapt to your system configuration – the mimic diagrams shown here are just examples.

The green power line (gray in illustration) in the mimic diagram shows the power flow through the UPS system. Active modules (inverter, rectifier, battery, static bypass switch, etc.) are framed in green and inactive modules are framed in black. Modules framed in red are inoperable or in an alarm condition.

In mimic diagrams for parallel systems, tap on the gray UPS to see the mimic diagram on UPS level.

NOTE: The mimic diagram only shows one battery breaker BB even if more battery breakers have been connected and configured for monitoring. If one or more of the monitored battery breakers are in the closed position, the BB on the mimic diagram will show as closed. If all of the monitored battery breakers are in the open position, the BB on the mimic diagram will show as open.

Example of Single UPS System – Dual Mains

Example of Simplified 1+1 Parallel System – Dual Mains

Example of Parallel System – Dual Mains

Alarm Status Symbol

The alarm status symbol (gray in illustration) in the top right corner of the display changes depending on the alarm status of the UPS system.

Green: No alarms present in the UPS system.
Blue: Informational alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log.
Yellow: Warning alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log.
Red: Critical alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log.

Menu Tree

  • Status

    • Input

    • Output

    • Bypass

    • Battery

    • Temperature

    • Parallel*

  • Logs

  • Control*

    • Operation mode

    • Inverter

    • Charger

    • Guided sequences

  • Configuration*

    • UPS

    • Output

    • Battery

    • High efficiency

    • Breakers

    • Contacts and relays

    • Network

    • Modbus

    • Reminder

    • General

    • Save/restore

    • Update status

    • Load shedding

  • Maintenance

    • Buzzer

    • Status LEDs

    • Breaker lamp

    • Battery*

    • Runtime calibration*

    • Battery replacement*

    • UPS report*

  • Statistics

  • About

  • Logout

  • Flag button – See Set the Display Language.

Some menus contain more submenus than described in this manual. These submenus are grayed out and are only for use by Schneider Electric to avoid unwanted load impacts. Other menu items can also be grayed out/not shown on the display if they are not relevant or not released yet for this particular UPS system.

Controller Section

NOTE: Remove the front panel to access the controller section.

Front View of the Controller Section

  1. Inverter ON/OFF buttons

  2. USB ports*

  3. Universal I/O*

  4. Modbus port*

  5. USB Micro-B port*

  6. Network port*

  7. Reset button*

  8. Input status LED*

  9. Inverter status LED*

  10. Output status LED*

  11. Bypass status LED*

  12. Battery status LED*

  13. Display power supply

  14. Display port

  15. Service port*

  16. For future use

  17. For future use

  18. PBUS 1*

  19. PBUS 2*

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.