990-5910G-018

温度センサー/湿度センサーの接続(オプション)

温度センサー/湿度センサー(AP9335TまたはAP9335TH)を、ネットワーク管理カードに接続することができます。

  1. 温度/湿度センサーを、ネットワーク管理カードのユニバーサルI/Oポートに接続します。
  2. ネットワーク管理インターフェイスを使用して、温度センサー/湿度センサーの設定を行います(設定したネットワーク管理インターフェイスへのアクセスを参照)。
  3. ステータス > 温度をタップして、温度センサー/湿度センサーの測定値を表示します。
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.