990-6363-001

Load Derating for UPS with IP52 Kit Installed

NOTICE
Risk of overheating
  • Galaxy VS IP52 UPS may have load deratings/temperature deratings.
  • Read all instructions in the installation manual before installing or working on this UPS.
Failure to follow these instructions can result in equipment damage.

380/400/415/480 V UPS

UPS rating Maximum continuous load at 30 °C (86 °F) Maximum continuous load at 35 °C (95 °F) Maximum continuous load at 40 °C (104 °F) Operating temperature and load derating

20 kW

20 kW

20 kW

20 kW

0 °C to 40 °C (32 °F to 104 °F): No derating.

30 kW

30 kW

30 kW

30 kW

0 °C to 40 °C (32 °F to 104 °F): No derating.

40 kW

40 kW

34 kW

30 kW

0 °C to 30 °C (32 °F to 86 °F): No derating;
30 °C to 40 °C (32 °F to 104 °F): Reduce load with 3% for every °C.
40 kW (N+1 power module)

40 kW

40 kW

40 kW

0 °C to 40 °C (32 °F to 104 °F): No derating.

50 kW

40 kW

34 kW

30 kW

40 kW maximum load on UPS. Output overload alarm settings need to be adjusted by Schneider Electric Service.
50 kW (N+1 power module)

50 kW

50 kW

50 kW

0 °C to 40 °C (32 °F to 104 °F): No derating.

60 kW

60 kW

60 kW

50 kW

0 °C to 35 °C (32 °F to 95 °F): No derating;
35 °C to 40 °C (95 °F to 104 °F): Reduce load with 3% for every °C.
60 kW (N+1 power module)

60 kW

60 kW

60 kW

0 °C to 40 °C (32 °F to 104 °F): No derating.

80 kW

80 kW

68 kW

50 kW

0 °C to 30 °C (32 °F to 86 °F): No derating;
30 °C to 40 °C (86 °F to 104 °F): Reduce load with 3% for every °C.
80 kW (N+1 power module)

80 kW

80 kW

80 kW

0 °C to 40 °C (32 °F to 104 °F): No derating.

100 kW

80 kW

68 kW

50 kW

80 kW maximum load on UPS. Output overload alarm settings need to be adjusted by Schneider Electric Service.
100 kW (N+1 power module)

100 kW

100 kW

84 kW

0 °C to 35 °C (32 °F to 95 °F): No derating;
35 °C to 40 °C (95 °F to 104 °F): Reduce load with 3% for every °C.

120 kW

120 kW

102 kW

84 kW

0 °C to 30 °C (32 °F to 86 °F): No derating;
30 °C to 40 °C (86 °F to 104 °F): Reduce load with 3% for every °C.

150 kW

120 kW

102 kW

84 kW

120 kW maximum load on UPS. Output overload alarm settings need to be adjusted by Schneider Electric Service.

200/208/220 V UPS

UPS rating Maximum continuous load at 30 °C (86 °F) Maximum continuous load at 35 °C (95 °F) Maximum continuous load at 40 °C (104 °F) Operating temperature and load derating

10 kW

10 kW

10 kW

10 kW

0 °C to 40 °C (32 °F to 104 °F): No derating.

15 kW

15 kW

15 kW

15 kW

0 °C to 40 °C (32 °F to 104 °F): No derating.

20 kW

20 kW

17 kW

15 kW

0 °C to 30 °C (32 °F to 86 °F): No derating;
30 °C to 40 °C (86 °F to 104 °F): Reduce load with 3% for every °C.

20 (N+1 power module)

20 kW

20 kW

20 kW

0 °C to 40 °C (32 °F to 104 °F): No derating.

25 kW

20 kW

17 kW

15 kW

20 kW maximum load on UPS. Output overload alarm settings need to be adjusted by Schneider Electric Service.

25 (N+1 power module)

25 kW

25 kW

25 kW

0 °C to 40 °C (32 °F to 104 °F): No derating.

30 kW

30 kW

30 kW

25 kW

0 °C to 35 °C (32 °F to 95 °F): No derating;
35 °C to 40 °C (95 °F to 104 °F): Reduce load with 3% for every °C.

40 kW

40 kW

34 kW

25 kW

0 °C to 30 °C (32 °F to 86 °F): No derating;
30 °C to 40 °C (86 °F to 104 °F): Reduce load with 3% for every °C.

40 (N+1 power module)

40 kW

40 kW

40 kW

0 °C to 40 °C (32 °F to 104 °F): No derating.

50 kW

40 kW

34 kW

25 kW

40 kW maximum load on UPS. Output overload alarm settings need to be adjusted by Schneider Electric Service.

50 (N+1 power module)

50 kW

50 kW

50 kW

0 °C to 35 °C (32 °F to 95 °F): No derating;
35 °C to 40 °C (95 °F to 104 °F): Reduce load with 3% for every °C.

60 kW

60 kW

51 kW

42 kW

0 °C to 30 °C (32 °F to 86 °F): No derating;
30 °C to 40 °C (86 °F to 104 °F): Reduce load with 3% for every °C.

75 kW

60 kW

51 kW

42 kW

60 kW maximum load on UPS. Output overload alarm settings need to be adjusted by Schneider Electric Service.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.