990-6511-001

Connect the Power Cables

  1. Lockout/Tagout the output switch.
  2. Connect the EGC from the UPS to the ground busbar.
  3. Remove the protective covers.
  4. Connect the EGC/ground from the ground busbar to the load.
  5. Connect the UPS output cables (L1, L2, L3).
  6. Connect the load cables (L1, L2, L3).
  7. Reinstall the protective covers.
  8. Attach the cables to the cable reliefs in the top and the bottom of the output switch box.
  9. Close the inner door and fasten with the three screws.
  10. Close the front door of the output switch box.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.