990-91260F-001

Install the Seismic Anchoring (Option)

  1. Mount the rear anchor(s) to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear anchor is ø14 mm.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.