DOCA0142EN-12

About the Document

Document Scope

The aim of this document is to provide the users, installers, and the maintenance personnel with the technical information and procedure needed to access and maintain the IFE Ethernet interface for one circuit breaker webpages.

Validity Note

This guide is valid for the IFE interface for use with:

  • MasterPacT™ MTZ circuit breakers with MicroLogic Active control unit

  • MasterPacT™ MTZ circuit breakers with MicroLogic X control unit

  • MasterPacT™ NT/NW circuit breakers

  • ComPacT™ NS 1600b - 3200

    circuit breakers
  • ComPacT™ NS 630b - 1600

    circuit breakers
  • PowerPacT™ P- and R-frame circuit breakers with MicroLogic A/E/P/H trip unit

  • ComPacT™ NSX circuit breakers with MicroLogic 5/6/7 trip unit

  • PowerPacT™ H-, J-, and L-frame circuit breakers with MicroLogic 5/6 trip unit

NOTE:
  • The information related to the new generation of ComPacT NS and PowerPacT P- and R-frame circuit breakers in this guide applies to ComPact NS and PowerPact P- and R-frame circuit breakers also. The exceptions are mentioned wherever applicable.

    The new ComPacT NS and PowerPacT P- and R-frame ranges are based on the same technical and dimensional architecture as that of ComPact NS and PowerPact P- and R-frame circuit breakers. The electrical and mechanical performances of these ranges are identical.

  • The information related to the new generation of and ComPacT NSX PowerPacT H-, J-, and L-frame circuit breakers in this guide applies to ComPact NSX and PowerPact H-, J-, and L-frame circuit breakers also. The exceptions are mentioned wherever applicable.

    The new ComPacT NSX and PowerPacT H-, J-, and L-frame ranges are based on the same technical and dimensional architecture as that of ComPact NSX and PowerPact H-, J-, and L-frame circuit breakers. The electrical and mechanical performances of these ranges are identical.

Online Information

The technical characteristics of the devices described in this guide also appear online. To access the information online, go to the Schneider Electric country website at www.se.com.

The information contained in this guide is likely to be updated at any time. Schneider Electric strongly recommends that you have the most recent and up-to-date version available on www.se.com/ww/en/download/.

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Product Related Cybersecurity Information

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
  • Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.
  • Disable unused ports/services and default accounts to help minimize pathways for malicious attackers.
  • Place networked devices behind multiple layers of cyber defenses (such as firewalls, network segmentation, and network intrusion detection and protection).
  • Use cybersecurity best practices (for example, least privilege, separation of duties) to help prevent unauthorized exposure, loss, modification of data and logs, or interruption of services.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Environmental Data

For product compliance and environmental information, refer to the Schneider Electric Environmental Data Program.

Available Languages of the Document

The document is available in these languages:

Related Documents for IEC Devices

Title of Documentation

Reference Number

Enerlin'X IFE – Ethernet Interface for One Circuit Breaker – Instruction Sheet

QGH13473

Enerlin'X IFE/EIFE - Ethernet Interface - Firmware Release Notes

DOCA0147EN

ULP (Universal Logic Plug) System - User Guide

MasterPacT, ComPacT, PowerPacT Circuit Breakers - Modbus Communication - User Guide

MasterPacT MTZ - MicroLogic Active Control Unit - User Guide

Breaker Communication and Isolation Module (BCIM) for MicroLogic Active Control Unit - User Guide

MasterPacT MTZ - MicroLogic X Control Unit - User Guide

MasterPacT MTZ Circuit Breakers with MicroLogic X Control Units - IEC 61850 Communication Guide

CET850 IEC 61850 Configuration Software - User's Manual

SEPED306025EN

Enerlin'X IO - Input/Output Application Module for One Circuit Breaker - User Guide

MasterPacT, ComPacT, PowerPacT - Cybersecurity Guide

EcoStruxure Cybersecurity Admin Expert Guide

CAE_UM_EN

To find documents online, visit the Schneider Electric download center (www.se.com/ww/en/download/).

Related Documents for UL/ANSI Devices

Title of Documentation

Reference Number

Enerlin'X IFE – Ethernet Interface for One Circuit Breaker – Instruction Sheet

QGH13473

Enerlin'X IFE/EIFE - Ethernet Interface - Firmware Release Notes

DOCA0147EN

ULP (Universal Logic Plug) System - User Guide

MasterPacT, ComPacT, PowerPacT Circuit Breakers - Modbus Communication - User Guide

MasterPacT MTZ - MicroLogic X Control Unit - User Guide

MasterPacT MTZ Circuit Breakers with MicroLogic X Control Units - IEC 61850 Communication Guide

CET850 IEC 61850 Configuration Software - User's Manual

SEPED306025EN

Enerlin'X IO - Input/Output Application Module for One Circuit Breaker - User Guide

MasterPacT, ComPacT, PowerPacT - Cybersecurity Guide

EcoStruxure Cybersecurity Admin Expert Guide

To find documents online, visit the Schneider Electric download center (www.se.com/ww/en/download/).

Information on Non-Inclusive or Insensitive Terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.