DOCA0142EN-12

EcoStruxure Power Commission Software

Overview

EcoStruxure TM Power Commission software helps you to manage a project as part of testing, commissioning, and maintenance phases of the project life cycle. The innovative features in it provide simple ways to configure, test, and commission the smart electrical devices.

EcoStruxure Power Commission software automatically discovers the smart devices and allows you to add the devices for an easy configuration. You can generate comprehensive reports as part of Factory Acceptance Test and Site Acceptance Test to replace your heavy manual work. Additionally, when the panels are under operation, any change of settings made can be easily identified by a yellow highlighter. This indicates the difference between the project and device values, and hence provides a system consistency during the operation and maintenance phase.

EcoStruxure Power Commission software enables the configuration of the following circuit breakers, modules, and accessories:

Circuit breaker ranges

Modules

Accessories

MasterPacT MTZ circuit breakers

  • MicroLogic Active control units

  • Communication interface modules: BCIM module, IFM interface, IFE interface, IFE server, and EIFE interface

  • ULP modules: FDM121 display *

MasterPacT MTZ circuit breakers

  • MicroLogic X control units

  • Communication interface modules: IFM interface, IFE interface, IFE server, and EIFE interface

  • ULP modules: IO module

    and FDM121 display *

M2C output module

  • MasterPacT NT/NW circuit breakers

  • ComPacT NS circuit breakers

  • PowerPacT P- and R-frame circuit breakers

  • MicroLogic trip units

  • Communication interface modules: BCM module, CCM module, BCM ULP module, IFM interface, IFE interface, and IFE server

  • ULP modules: IO module and FDM121 display *

M2C and M6C output modules

  • ComPacT NSX circuit breakers

  • PowerPacT H-, J-, and L-frame circuit breakers

  • MicroLogic trip units

  • Communication interface modules: BSCM or BSCM Modbus SL/ULP module, IFE interface, IFM interface, and IFE server

  • ULP modules: IO module and FDM121 display *

SDTAM and SDx output modules

For more information, refer to the EcoStruxure Power Commission Software Online Help.

Click here to download the latest version of EcoStruxure Power Commission software.

Key Features

EcoStruxure Power Commission software performs the following actions for the supported devices and modules:

  • Create projects by device discovery.

  • Save the project in the EcoStruxure Power Commission cloud for reference.

  • Upload standard protection settings to the device and download standard protection settings from the device.

  • Compare the standard protection settings between the project and the device.

  • Generate and print the device standard protection settings report.

  • View the logs and maintenance information.

  • View the alarm details.

  • Check the system firmware compatibility status.

  • Update to the latest device firmware.

  • Perform automatic trip curve tests with preconfigured or custom test points.

  • Perform arc energy reduction tests in compliance with NEC 240.87(C).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.