DOCA0142EN-12

Date and Time

Description

The Date and Time page allows you:

  • To manually set the date and time of the circuit breaker connected to the IFE interface.

  • To automatically synchronize the date and time of the circuit breaker to the IFE interface time.

  • To periodically check the synchronization at specified interval of time.

List of Parameters in Date and Time Configuration

Parameter

Description

Manual

Allows you to select the manual date and time setting of the circuit breaker connected to the IFE interface. This option is disabled when Automatic (SNTP) is selected.

Date

Allows you to set the present date manually in the format YYYY-MM-DD.

Time

Allows you to set the present time manually in the format hh:mm:ss.

Automatic (SNTP)

Allows you to enable the automatic time setting of the circuit breaker connected to the IFE interface. This option is disabled when Manual is selected.

Poll Interval

Allows you to enter the poll interval in hours that ranges from 1 through 63.

Obtain Servers Automatically via DHCP/BOOTP

Allows you to enable the check box that obtains the server address from DHCP or BOOTP.

Primary SNTP/NTP server

Allows you to enter the primary SNTP server address.

Secondary SNTP/NTP server

Allows you to enter the secondary SNTP server address.

Apply

Allows you to automatically synchronize the time of the circuit breaker connected to the IFE interface with the IFE interface time.

Cancel

Allows you to clear the synchronization of the circuit breaker connected to the IFE interface.

Setting the IFE Interface Date and Time Manually

Step

Action

Result

1

From the IFE menu bar, click Configuration & Settings.

Opens the Configuration & Settings menu.

2

In the General submenu, click Date and Time and then select Manual from the Date/Time Settings.

The parameters for date and time settings is available.

3

Enter the date in the format YYYY-MM-DD.

Sets the date of the IFE interface manually.

4

Enter the time in the format hh:mm:ss.

Sets the time of the IFE interface manually.

5

Click Apply.

The date and time of IFE interface is set.

Setting the IFE interface Date and Time Automatically with SNTP

Step

Action

Result

1

From the IFE menu bar, click Configuration & Settings.

Opens the Configuration & Settings menu.

2

In the General submenu, click Date and Time and then select Automatic (SNTP) from the Date/Time Settings.

The circuit breaker connected to the IFE interface is selected by default for date and time synchronization.

3

Enter the poll time in the Poll Interval box.

The entered time is updated.

4

Select to obtain SNTP server automatically via DHCP/BOOTP.

The SNTP server address is obtained automatically.

5

Enter the primary and secondary server address in the Primary SNTP/NTP server and Secondary SNTP/NTP server box.

The entered SNTP server address is updated.

8

Click Apply.

The date and time of the circuit breaker get synchronized with the IFE interface time.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.