DOCA0142EN-12

Ethernet Configuration (Dual Port)

Ethernet

Parameter

Description

Settings

MAC address

A unique media access control address of an IFE interface. The MAC address is written on the label which is placed on the side of the IFE interface.

Frame format

Used to select the format for data sent over an Ethernet connection.

NOTE: Whenever the frame format settings are changed, restart the device to implement the changes.
  • Ethernet II

  • 802.3

  • Auto (default setting)

Ethernet Port Control

Parameter

Description

Settings

Speed and mode for Port #1

Used to define the physical Ethernet connection speed and transmission mode for Ethernet port 1.

Auto-negotiation (default setting)

Speed and mode for Port #2

Used to define the physical Ethernet connection speed and transmission for Ethernet port 2.

Auto-negotiation (default setting)

Broadcast Storm Protection

Parameter

Description

Settings

Level

Defines the broadcast storm protection level. The level value corresponds to a committed information rate (CIR) value, that is, the amount of traffic entering the switch port from which the storm protection drops entering the broadcast traffic.

NOTE: If the level value is changed, you are prompted to restart the device to implement changes.

Broadcast storm protection level:

  • 1: Highest (1000)

  • 2: High (2000)

  • 3: Medium-High (3000)

  • 4: Medium-Low (4000), Default setting

  • 5: Low (5000)

  • 6: Lowest (6000)

NOTE: The level value corresponds to the committed information rate.

Committed information rate

Defines the read-only value of the broadcast storm protection level.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.