DOCA0142EN-12

Schematics with MasterPacT MTZ Circuit Breakers

Description

The IFE interface is connected to the MasterPacT MTZ circuit breaker with:

  • MicroLogic Active control unit through its ULP port module or COM terminal block.

  • MicroLogic X control unit through its ULP port module

For more information, refer to the DOCA0093•• ULP (Universal Logic Plug) System - User Guide.

ULP Connection

NOTICE
HAZARD OF EQUIPMENT DAMAGE
  • Never connect an Ethernet device to a RJ45 ULP port.
  • The RJ45 ULP ports of IFE interface are for ULP modules only.
  • Any other use can damage the IFE interface or the device connected to the IFE interface.
  • To check if a ULP module is compatible with the RJ45 ULP ports of IFE interface, refer to the DOCA0093•• ULP (Universal Logic Plug) System - User Guide.
Failure to follow these instructions can result in equipment damage.

All the connection configurations require the RJ45 plug/plug ULP cord.

When the second RJ45 ULP port is not used, it must be closed with an ULP line termination.

A

RJ45 plug/plug ULP cord or circuit breaker BCM ULP cord

B

ULP line termination

Connection of the IFE Interface to a MasterPacT MTZ Circuit Breaker

Connect the IFE interface to the ULP port module on a MasterPacT MTZ circuit breaker by using the ULP cord.

A

IFE Ethernet interface for one circuit breaker

B

ULP line termination

C

RJ45 plug/plug ULP cord

D

ULP port module

E

MasterPacT MTZ fixed circuit breaker

Connection of the IFE Interface to a MasterPacT MTZ Circuit Breaker with MicroLogic Active Control Unit

Connect the IFE interface to the MasterPacT MTZ circuit breaker with MicroLogic Active control unit through:

  • ULP port module and RJ45 plug/plug ULP cord.

  • COM terminal block and circuit breaker BCM ULP cord.

A

IFE Ethernet interface for one circuit breaker

B

ULP line termination

C

RJ45 plug/plug ULP cord

D

Circuit breaker BCM ULP cord

E

ULP port module

F

COM terminal block

G

BCIM module

H

MicroLogic Active control unit

I

MasterPacT MTZ circuit breaker

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.