DOCA0142EN-12

User Accounts

Description

The IFE interface users are assigned with user names and passwords. Each user belongs to a group, and each group has access rights to the IFE webpages assigned by the IFE interface administrator.

NOTE: There are two pre-defined user accounts:
  • Administrator (the default password is Gateway)

  • Guest (the default password is Guest)

Groups

To change the group name, enter a new name in one of the group text boxes.

NOTE: The administrator group name cannot be changed.

Password

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

A password can be changed on the User Accounts webpage. A password is composed of 0 to 11 characters. It is case-sensitive and the allowed characters are:

  • Digits from 0 to 9

  • Letters from a to z

  • Letters from A to Z

  • Special characters as *, /, \, and so on

NOTE: Password with eleven asterisks (***********) is not allowed.

Users

Parameter

Description

Name

Enter a name (1 to 15 characters) for a new user.

NOTE: User names are case-sensitive and can contain only alphanumeric characters.

Password

Enter a password (0 to 11 characters) for a new user.

Email ID

Enter a valid email address for the selected name.

Group

Select a group for the new user.

Language

Select the language for the new user and click Apply to view the webpages in the selected language.

NOTE: When the administrator switches to a different language for the user account, make sure to refresh the webpage manually to display the webpages in a selected language.
NOTE: The maximum number of user-defined accounts are 11.

IFE Interface Accounts and Passwords

Accounts

Password

Administrator

Gateway

Guest

Guest

User-defined accounts (11 accounts possible)

User-defined passwords

NOTE:
  • You can change your password.

  • If you forget the password, contact your local Schneider Electric service team for retrieving the password.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.