DOCA0084EN-13

Redundancy-RSTP

Description

The REDUNDANCY-RSTP page allows you to set the RSTP bridge and RSTP port details.

The users with Installer or Engineer roles can change the Redundancy-RSTP settings.

For REDUNDANCY-RSTP settings, after clicking Apply Changes, a dialog is displayed for confirmation to restart the IFE server to apply the new settings:

  • Click Yes to restart the IFE server and apply the setting changes.

  • Click No to cancel the setting modifications and return to the last saved settings.

Navigation to the REDUNDANCY-RSTP Page

To view the REDUNDANCY-RSTP page, click SETTINGS > COMMUNICATION > REDUNDANCY-RSTP.

RSTP Settings

Setting

Description

Enable

Allows you to enable RSTP feature (disabled by default).

RSTP Bridge Settings

Setting

Description

Value

Bridge Priority

Allows you to select bridge priority.

  • Setting range: 0...61440

  • Default setting: 32768

Bridge Hello Time

Allows you to enter bridge hello time.

  • Setting range: 1...2 s

  • Default setting: 2 s

Bridge Max Age Time

Allows you to enter bridge maximum age time.

  • Setting range: 6...40 s

  • Default setting: 40 s

Transmit Hold Count

Allows you to enter the transmit hold count.

  • Setting range: 3...100 s

  • Default setting: 6 s

Bridge Forward Delay

Allows you to enter bridge forward delay.

  • Setting range: 4...30 s

  • Default setting: 21 s

RSTP Port 1 and 2 Settings

Settings

Description

Value

RSTP setting mode

Allows you to select the RSTP setting mode:

  • Select Automatic (default setting) to set RSTP port 1 and 2 automatically.

  • Select Manual to set manually the RSTP port 1 and 2 parameters (port priority and port cost).

–

Port 1 and 2 Priority

Allows you to select manually port 1 and 2 priority.

  • Setting range: 0...240

  • Default setting: 128

Port 1 and 2 Cost

Allows you to enter manually the port 1 and 2 cost.

  • Setting range: 1...200000000

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.