DOCA0084EN-13

Schematics with MasterPacT MTZ Circuit Breakers

Description

The IFE server is connected to the MasterPacT MTZ circuit breaker with:

  • MicroLogic Active control unit through its ULP port module or COM terminal block.

  • MicroLogic X control unit through its ULP port module.

For more information on the ULP system and its components, refer to the DOCA0093•• ULP (Universal Logic Plug) System - User Guide.

ULP Connection

NOTICE
HAZARD OF EQUIPMENT DAMAGE
  • Never connect an Ethernet device to an RJ45 ULP port.
  • The RJ45 ULP ports of IFE server are for ULP modules only.
  • Any other use can damage the IFE server or the device connected to the IFE server.
  • To check if an ULP module is compatible with the RJ45 ULP ports of IFE server, refer to the DOCA0093•• ULP (Universal Logic Plug) System - User Guide.
Failure to follow these instructions can result in equipment damage.

All the connection configurations require the RJ45 plug/plug ULP cord.

When the second RJ45 ULP port is not used, it must be closed with an ULP line termination.

A

RJ45 plug/plug ULP cord or circuit breaker BCM ULP cord

B

ULP line termination

Connection of the IFE Server to a MasterPacT MTZ Circuit Breaker with MicroLogic X Control Unit

Connect the IFE server to the ULP port module on a MasterPacT MTZ circuit breaker with MicroLogic X control unit by using the ULP cord.

A

IFE Ethernet switchboard server

B

ULP line termination

C

RJ45 plug/plug ULP cord

D

ULP port module

E

MasterPacT MTZ fixed circuit breaker with MicroLogic X control unit

Connection of the IFE Server to a MasterPacT MTZ Circuit Breaker with MicroLogic Active Control Unit

Connect the IFE server to the MasterPacT MTZ circuit breaker with MicroLogic Active control unit through:

  • ULP port module and RJ45 plug/plug ULP cord.

  • COM terminal block and circuit breaker BCM ULP cord.

A

IFE Ethernet switchboard server

B

ULP line termination

C

RJ45 plug/plug ULP cord

D

Circuit Breaker BCM ULP cord

E

ULP port module

F

COM terminal block

G

BCIM module

H

MicroLogic Active control unit

I

MasterPacT MTZ circuit breaker

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.