DOCA0084EN-13

IP Configuration

IPv4 Configuration

Parameter

Description

Settings

Obtain an IP address automatically using

Used to select the mode for assigning the IPv4 parameters set. Obtain IPv4 parameters automatically using BOOTP or DHCP.

NOTE: While using a legacy DHCP server, the device name must be limited to 16 characters.
  • DHCP (Factory setting)

  • BOOTP

Manual IP address

Used to enter the static IP address of an IFE server.

Manual Subnet mask

Used to enter the Ethernet IP subnet mask address of your network.

Manual Default gateway

Used to enter the gateway (router) IP address used for wide area network (WAN) communication.

IPv6 Configuration

Parameter

Description

Settings

Enable IPv6

Defines the IPv6 configuration.

Enabled (Factory setting)

NOTE: The setting is unavailable to edit.

Link local address

Used to open the IFE webpage for future use.

NOTE: In the URL address box, use [ ] brackets to enter the link local address.

DNS

Parameter

Description

Setting

Obtain DNS address automatically

Defines the dynamic behavior of the DNS server address configuration. Used to obtain the IP address from the DNS server automatically.

NOTE: Domain name system (DNS) is the naming system for computers and devices connected to a local area network (LAN) or the Internet.

Disabled when manual setting is selected.

Manual Primary server address

Defines the IPv4 address of the primary DNS server.

Manual Secondary server address

Defines the IPv4 address of the secondary DNS server. Used to perform a DNS resolution when the resolution fails with the primary DNS server.

Duplicate IP Address Detection

While connected to your network, the IFE server publishes its IP address. To avoid any duplicate IP address conflicts, the IFE server uses the address resolution protocol (ARP) to see if any other device on your network is using the same IP address. The following table explains how the IFE server handles a duplicate IP address when it is detected.

Duplicate IP Address Scenario

Scenario

Duplicate IP Detected

Network Status LED

Ethernet link detected

Reverts to the default IP address, subnet mask, and gateway address. ARP requests are sent every 15 seconds until the IP address is available. IFE server uses the IP address when it is available,

Steady red

Manual address change

Reverts to the default IP address, subnet mask, and gateway address. The ARP requests are sent every 15 seconds until the IP address is available. The IFE server uses the IP address when it is available.

Steady red

Receives an ARP request

If more than one ARP is detected within 10 seconds, initiate the process to reacquire the IP.

OFF

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.