DOCA0084EN-13

Device Control

Reset Commands

The Device Control page allows you to execute one or more reset commands per device type.

From the Control menu, in the Device Control submenu, on the device list, select the device and click Reset. Select an Operation in the Resets list to reset.

Application Control

The Device Control page allows you to control the following applications remotely:

  • Breaker application

  • IO application

By default, this feature is disabled in IFE server.

Password Management

When the application control operation is performed, an Authorization Required dialog box appears in the IFE webpage. Enter the password in the Authorization Required dialog box to perform the application control operation.

The password is required for:

  • MasterPacT MTZ circuit breaker with MicroLogic X control units.

  • MasterPacT NT/NW, PowerPacT P- and R-frame, or ComPacT NS circuit breaker with BCM ULP.

  • ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breaker with BSCM.

The following operations in the Device Control page require a password:

Control

Operation

Availability

Breaker/Switch disconnector (BCM-OF/SD)

Open/Close/Reset

ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breaker with BSCM

Open/Close

  • MasterPacT MTZ circuit breaker with MicroLogic X control units

  • MasterPacT NT/NW, ComPacT NS, or PowerPacT H-, J-, and L-frame circuit breakers with BCM ULP

Light

On/Off

IO 1 or IO 2

Load

On/Off

IO 1 or IO 2

Reset input counters

I1 I2 I3 I4 I5 I6

IO 1

#I1 #I2 #I3 #I4 #I5 #I6

IO 2

Reset output counters

O1 O2 O3

IO 1

#O1 #O2 #O3

IO 2

User-defined output control

On/Off

IO 1 or IO 2

Enable Application Control in IFE Server

Follow the below procedure to enable the Application Control feature in IFE server.

NOTE: The application control feature can only be enabled when the user is logged in as an administrator.

Step

Action

Result

1

Press the test button on the front face of the IFE server for 10–15 s.

NOTE: Do not press the test button less than 10 s or more than 15 s.

Initiates the application control feature.

2

After 15 s, IFE server initiates the application control feature.

The feature disclaimer window is available continuously for 5 min. The module status LED starts blinking continuously for 5 min (1 s ON, 1 s OFF) once the test button is released.

3

Access the IFE webpage and login as an administrator.

The administrator login to the IFE webpage.

4

From the Configuration & Settings menu, click Webpage Access.

The Administrator reads the disclaimer and chooses either the option I Understand the risks/Apply or Continue to disable.

The application control feature disclaimer is:

By accepting this disclaimer, you are directed to webpage access which enables you to control several applications remotely. It is highly recommended that the administrator modify the default administrator password. By using, you are agreeing to indemnify and hold harmless Schneider Electric for and from any claims, losses, demands, lawsuits, and damages that are a result of direct or indirect use of this application control feature by reason of any act or emission which the user commits.

The disclaimer page is available in the language selected by the administrator.

5

Select I Understand the risks/Apply.

The application control feature is now enabled for the administrator. The breaker application and IO application are enabled in the webpage access for providing access to the other user groups.

6

Select Continue to disable.

The application control feature is disabled. The breaker application and IO application are disabled in the webpage access.

Breaker Application

From the Device Control page, in the Breaker Application, the authorized group can perform the following operations:

Control

Status

Operation

Availability

Breaker

Open/Close/Tripped/NA

Open/Close/Reset

ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breaker with BSCM

Open/Close

  • MasterPacT MTZ circuit breaker with MicroLogic X control units

  • MasterPacT NT/NW, ComPacT NS, or PowerPacT P- and R-frame circuit breaker or switch disconnector with BCM ULP

NOTE: A message confirms that the command is successfully sent. It does not confirm whether the complete operation is successful.

IO Application

From the Device Control page, in the IO Application, the authorized group can perform the following operations:

Control

Status

Operation

Availability

Reset input counters

I1 I2 I3 I4 I5 I6

IO 1

#I1 #I2 #I3 #I4 #I5 #I6

IO 2

Reset output counters

O1, O2, O3

IO 1

#O1 #O2 #O3

IO 2

Light control

ON or OFF

ON / OFF

IO 1 or IO 2

Load control

ON or OFF

ON / OFF

IO 1 or IO 2

User-defined output control

ON or OFF

ON / OFF

IO 1 or IO 2

NOTE:
  • The IO application control is possible only when the IO module is connected to a circuit breaker.

  • The light and the load control are available when the application rotary switch of IO 1 or IO 2 is in position 4.

  • The user-defined output control is available only when the user-defined output has been assigned with Ecoreach software.

  • If the input is assigned as a pulse counter, the operation is P1, P2, P3, P4, P5, and P6 for IO 1. For IO 2, the pulse counter operation is #P1, #P2, #P3, #P4, #P5, and #P6.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.