DOCA0148EN-08

Firmware Version 005.001.000

Security Updates

Enhanced the following Cybersecurity features:

  • Enabled the HTTPS mode for the web interface.

  • Enabled the FTPS mode for file import.

  • Added the Syslog logging service feature.

  • Revised the user management configuration rules according to the Role Base Access Control (RBAC) strategy.

  • Added RBAC for MasterPacT MTZ and ComPacT NSX with MicroLogic 5, 6, and 7 trip units.

  • Enabled automatic export of datalog file.

  • Enabled compatibility with EcoStruxure Cybersecurity Admin Expert software.

    • Added Device Specific Settings (DSS) feature that enables the IFE or EIFE interface configurations to be tailored for each individual device.

    • Added signature verification feature to validate the security configuration files received from EcoStruxure Cybersecurity Admin Expert software.

  • Added the Machine-to-Machine (M2M) communication for Modbus communication.

  • Enhanced the policies of password security.

New Features

The following features are added:

  • Enhanced firmware upgrade feature.

  • Improved design for the webpage interface.

  • IEC 61850 communication protocol which is compatible with CET850 configuration software.

  • Rapid Spanning Tree Protocol (RSTP).

  • Enhanced the Simple Network Time Protocol (SNTP) with the Network Time Protocol (NTP).

  • Integration of BSCM Modbus SL/ULP module.

  • Reset security administrator password.

Known Issues

The firmware version 005 does not support the following features as compared to the firmware version 003:

  • Firmware version 005 supports less devices as compared to the firmware version 003. For more information, refer to the list of supported devices with the firmware version 005 and the firmware version 003 in the Enerlin'X IFE - Ethernet Switchboard Server - User Guide.

  • Display of the IO module input/output configuration.

  • Adding remote devices.

  • Trending graphs.

  • Data logging for serial devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.