7EN02-0421-03

IM400N Configuration

You need to perform IM400N configuration to enable the device to work as expected.

Perform the following network settings on the IM400N to enable compatibility with the device:

NOTE: You need to perform these settings again when you perform factory reset on the IM400N.

  1. Select Menu > Settings > Network.
  2. Set the value for the following network parameters and save:
    Parameter Value
    App Power C. or Control C.
    Locating IFL12
    V. Adapt None or PHT1000
    NOTE: See IM400N user manual for information on modifying parameters.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.