7EN02-0423-03

Alarm configuration

You can configure the insulation alarm threshold and delay, preventive insulation alarm threshold and delay, and injection detection to suit to the electrical applications you want to monitor.

You can access the device alarm parameters by selecting Menu > Settings > Ins.Alarm.

The alarm parameters are:

  • Ins. Alarm

  • Ins. Al. Delay

  • Prev. Alarm

  • Prev. Al. Del.

  • Disconnect. Inj.

To modify the parameter value, see Parameter modification using the display.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.