7EN02-0423-03

Information icons

Icons in the information area of the LCD display provide information such as what menu is selected and the insulation alarm status.

The following table is profiled. Check for row profiling before updating any content
Icon Description
Main menu
  • System resistance (in the absence of an insulation fault)

  • Measurement parameters menu

  • Monitoring menu

  • System impedance

  • System resistance as primary record in Logging page

  • Setup Summary

Fault log menu
Trend menu
Setting parameters menu and submenu
Display language selection menu
Product identification
  • Indication of an insulation alarm

  • Indication of a preventive insulation alarm

  • Indication of a transient alarm

  • Indication of product status

Check for IFL12H row profiling

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.